Other Parts Discussed in Thread: EK-TM4C1294XL
Hello,
I just upgraded to TivaWare 2.1.3.156, and my application which runs on a EK-TM4C1294XL just stopped receiving CAN packets.
My application is based on the examples/peripherals/can/simple_rx.c, and after upgrading to 2.1.3.156, I only receive the first CAN packet.
Excerpt of the code:
void motorCAN_Init(void)
{
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_GPIOPinConfigure(GPIO_PA0_CAN0RX);
MAP_GPIOPinConfigure(GPIO_PA1_CAN0TX);
MAP_GPIOPinTypeCAN(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
MAP_CANInit(CAN0_BASE);
MAP_CANBitRateSet(CAN0_BASE, TM4C129FREQ, 1000000);
CANIntRegister(CAN0_BASE, CAN0IntHandler);
// Enable interrupts on the CAN peripheral.
MAP_CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR);// | CAN_INT_STATUS);
MAP_IntEnable(INT_CAN0);
MAP_CANEnable(CAN0_BASE);
g_sCAN0RxMessage.ui32MsgID = CAN0RXID;
g_sCAN0RxMessage.ui32MsgIDMask = 0;
g_sCAN0RxMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER;
g_sCAN0RxMessage.ui32MsgLen = sizeof(g_sRXMsgData);
g_sCAN0RxMessage.pui8MsgData = (uint8_t *)&g_sRXMsgData;
MAP_CANMessageSet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, MSG_OBJ_TYPE_RX);
g_sCAN0TxMessage.ui32MsgID = CAN0TXID;
g_sCAN0TxMessage.ui32MsgIDMask = 0;
g_sCAN0TxMessage.ui32Flags = MSG_OBJ_NO_FLAGS;
g_sCAN0TxMessage.ui32MsgLen = sizeof(g_sTXMsgData);
g_sCAN0TxMessage.pui8MsgData = (uint8_t *)&g_sTXMsgData;
}
static void CAN0IntHandler(void)
{
uint32_t ui32Status;
// Read the CAN interrupt status to find the cause of the interrupt
ui32Status = MAP_CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);
// If this was a status interrupt acknowledge it by reading the CAN
// controller status register.
if (ui32Status == CAN_INT_INTID_STATUS)
{
ui32Status = MAP_CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
g_ui32ErrFlag |= ui32Status;
// Send error to external handler
if (g_ui32ErrFlag)
motorCAN_ISRHook(g_ui32ErrFlag | CAN_HOOK_ERROR_MASK);
MAP_CANIntClear(CAN0_BASE, CAN_INT_INTID_STATUS);
}
// Check if the cause is message object RXOBJECT, which we are using
// for receiving messages.
else if (ui32Status == RXOBJECT)
{
MAP_CANIntClear(CAN0_BASE, RXOBJECT);
g_ui32RXMsgCount++;
g_ui32ErrFlag = 0;
// Set flag to indicate received message is pending.
motorCAN_ISRHook(ui32Status);
}
}
// Hook which runs on ISR context!!
void motorCAN_ISRHook(uint32_t ui32Status)
{
if (xCANParserTaskHandle != NULL)
{
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
xTaskNotifyFromISR(xCANParserTaskHandle, ui32Status, eSetValueWithOverwrite, &xHigherPriorityTaskWoken);
portYIELD_FROM_ISR(xHigherPriorityTaskWoken);
}
}
uint32_t motorCAN_ReceiveMessage(uint8_t *pui8RXBuff)
{
ROM_CANMessageGet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, false);
for (int i=0; i<g_sCAN0RxMessage.ui32MsgLen; i++) pui8RXBuff[i] = g_sCAN0RxMessage.pui8MsgData[i];
return g_sCAN0RxMessage.ui32MsgLen;
}
// task while:
ui32Notification = ulTaskNotifyTake(pdTRUE, portMAX_DELAY);
// Get the CAN message
tFbkMsg sFbkMsg;
sFbkMsg.length = motorCAN_ReceiveMessage(sFbkMsg.data);
At first glance, it seems that the new CANIntClear, does not really clear the interrupt.
When I revert the changes made by the new TivaWare to CANIntClear, it works.
What can be the issue?