Part Number: TM4C129XNCZAD
Tool/software: Code Composer Studio
Hi, I have a problem using ethernet driver, in particular related to the clock configuration.
With these settings, ethernet worked fine:
SysCtlMOSCConfigSet(SYSCTL_MOSC_HIGHFREQ);
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000);
SysCtlVCOGet(SYSCTL_XTAL_25MHZ, &ui32PLLRate);
But I had many problems with all other peripherals, so I had to set the clock in this way:
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_OSC), 25000000); // 25MHz
But now ethernet doesn't work anymore.....in the function that initializes ethernet, there is also a call to lwIPInit(g_ui32SysClock, pui8MACArray, parIP.IP_address, parIP.IP_netmask, parIP.IP_gateway, IPADDR_USE_STATIC).... maybe the problem is in this call? Can anyone help me with this settings please? I have to set the sysclock @25MHz, but the ethernet driver must work anyway.
Thank you
Cristina