Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: Trouble with SSI3 slave conversion to SSI1

Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: SYSBIOS

Tool/software: TI-RTOS

I have a TIVA TM4c1294NCPT launchpad and have SSI2 setup as a master SPI communicating to SSI3 slave SPI on the same development board with jumper wires.  This has worked well for me.  Now I need to change the slave SPI from SSI3 to SS1 but I can't seem to get this to work. My jumper wire setup is as follows:
Generic setup:   SSI2Clk -> SSIxCLK, SSI2Fss -> SSIxFss, SSI2Data1->SSIxData0, SSI2Data0->SSIxData1,
SSI2->SSI3:      PD3->PQ0, PD2->PQ1, PD0->PQ2, PD1->PQ3
SSI2->SSI1:      PD3->PB5, PD2->PB4, PD0->PE4, PD1->PE5
The program compiles and the master seems to issue messages OK.  When the SPI slave is SSI3, the messages are received.  My SPI slave task is as follows:

void SPIserver(UArg arg0, UArg arg1)
{
    SPI_Handle serverSpi;
    SPI_Params serverSpiParams;
    SPI_Transaction serverTransaction;
    bool ServertransferOK;

    /* Initialize SPI handle with slave mode */
    SPI_Params_init(&serverSpiParams);
    serverSpiParams.mode = SPI_SLAVE;
    serverSpiParams.bitRate = 12500000;
    serverSpiParams.transferMode = SPI_MODE_BLOCKING;
    serverSpiParams.frameFormat = SPI_POL0_PHA1; // polarity and phase == SPI_POL0_PHA0, SPI_POL0_PHA1, SPI_POL1_PHA0, SPI_POL1_PHA1
    //serverSpiParams.transferTimeout = SPI_WAIT_FOREVER;
    serverSpiParams.dataSize = 10;


    serverSpi = SPI_open(Board_SPI3, &serverSpiParams);

    if (serverSpi == NULL) {
        System_abort("Error initializing SPI\n");
    }
    else
    {
        System_printf("Server SPI initialized\n");
    }

    while(1)
    {
        //Step 1: receive new SPI data
        serverTransaction.count = SPI_MSG_LENGTH;
        serverTransaction.txBuf = NULL;
        serverTransaction.rxBuf = (Ptr)serverRxBuffer;
        ServertransferOK = SPI_transfer(serverSpi, &serverTransaction);
    }
}


This checks out OK.  Now when I change my hook-up wires from SSI3 to SSI1 as noted earlier and change "Board_SPI3" to ""Board_SPI1" in SPI_open() in the above program, my slave SPI stays in a blocking mode.  The constant definitions are as follows:
#define Board_SPI1                  EK_TM4C1294XL_SPI1
#define Board_SPI2                  EK_TM4C1294XL_SPI2
#define Board_SPI3                  EK_TM4C1294XL_SPI3

What am I missing.  Is there some other configuration that I need to configure for SSI1 that I didn't for SSI3?  This is similar to a post about a SPI_transfer crash reported a few days ago by digvijay khambe.  Any help would be great appreciated.  Please find the relavent code posted below.  Thank you!


/*!
 *  @def    EK_TM4C1294XL_SPIName
 *  @brief  Enum of SPI names on the EK_TM4C1294XL dev board
 */
typedef enum EK_TM4C1294XL_SPIName {
    EK_TM4C1294XL_SPI1 = 0,
    EK_TM4C1294XL_SPI2,
    EK_TM4C1294XL_SPI3,

    EK_TM4C1294XL_SPICOUNT
} EK_TM4C1294XL_SPIName;







/*
 *  =============================== SPI ===============================
 */
/* Place into subsections to allow the TI linker to remove items properly */
#if defined(__TI_COMPILER_VERSION__)
#pragma DATA_SECTION(SPI_config, ".const:SPI_config")
#pragma DATA_SECTION(spiTivaDMAHWAttrs, ".const:spiTivaDMAHWAttrs")
#endif

#include <ti/drivers/SPI.h>
#include <ti/drivers/spi/SPITivaDMA.h>

SPITivaDMA_Object spiTivaDMAObjects[EK_TM4C1294XL_SPICOUNT];

#if defined(__TI_COMPILER_VERSION__)
#pragma DATA_ALIGN(spiTivaDMAscratchBuf, 32)
#elif defined(__IAR_SYSTEMS_ICC__)
#pragma data_alignment=32
#elif defined(__GNUC__)
__attribute__ ((aligned (32)))
#endif
uint32_t spiTivaDMAscratchBuf[EK_TM4C1294XL_SPICOUNT];

const SPITivaDMA_HWAttrs spiTivaDMAHWAttrs[EK_TM4C1294XL_SPICOUNT] = {
   {
         .baseAddr = SSI1_BASE,
        .intNum = INT_SSI1,
        .intPriority = (~0),
        .scratchBufPtr = &spiTivaDMAscratchBuf[0],
        .defaultTxBufValue = 0,
        .rxChannelIndex = UDMA_SEC_CHANNEL_SSI1RX,
        .txChannelIndex = UDMA_SEC_CHANNEL_SSI1TX,
        .channelMappingFxn = uDMAChannelAssign,
        .rxChannelMappingFxnArg = UDMA_CH10_SSI1RX,
        .txChannelMappingFxnArg = UDMA_CH11_SSI1TX
   },
   {
        .baseAddr = SSI2_BASE,
        .intNum = INT_SSI2,
        .intPriority = (~0),
        .scratchBufPtr = &spiTivaDMAscratchBuf[1],
        .defaultTxBufValue = 0,
        .rxChannelIndex = UDMA_SEC_CHANNEL_UART2RX_12,
        .txChannelIndex = UDMA_SEC_CHANNEL_UART2TX_13,
        .channelMappingFxn = uDMAChannelAssign,
        .rxChannelMappingFxnArg = UDMA_CH12_SSI2RX,
        .txChannelMappingFxnArg = UDMA_CH13_SSI2TX
    },
    {
        .baseAddr = SSI3_BASE,
        .intNum = INT_SSI3,
        .intPriority = (~0),
        .scratchBufPtr = &spiTivaDMAscratchBuf[2],
        .defaultTxBufValue = 0,
        .rxChannelIndex = UDMA_SEC_CHANNEL_TMR2A_14,
        .txChannelIndex = UDMA_SEC_CHANNEL_TMR2B_15,
        .channelMappingFxn = uDMAChannelAssign,
        .rxChannelMappingFxnArg = UDMA_CH14_SSI3RX,
        .txChannelMappingFxnArg = UDMA_CH15_SSI3TX
    }
};

const SPI_Config SPI_config[] = {
    {
        .fxnTablePtr = &SPITivaDMA_fxnTable,
        .object = &spiTivaDMAObjects[0],
        .hwAttrs = &spiTivaDMAHWAttrs[0]
    },
    {
        .fxnTablePtr = &SPITivaDMA_fxnTable,
        .object = &spiTivaDMAObjects[1],
        .hwAttrs = &spiTivaDMAHWAttrs[1]
    },
    {
        .fxnTablePtr = &SPITivaDMA_fxnTable,
        .object = &spiTivaDMAObjects[2],
        .hwAttrs = &spiTivaDMAHWAttrs[2]
    },
    {NULL, NULL, NULL}
};

/*
 *  ======== EK_TM4C1294XL_initSPI ========
 */
void EK_TM4C1294XL_initSPI(void)
{

    /* SSI1 */
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);

    GPIOPinConfigure(GPIO_PB5_SSI1CLK);
    GPIOPinConfigure(GPIO_PB4_SSI1FSS);
    GPIOPinConfigure(GPIO_PE4_SSI1XDAT0);
    GPIOPinConfigure(GPIO_PE5_SSI1XDAT1);

    GPIOPinTypeSSI(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
    GPIOPinTypeSSI(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5);


    /* SSI2 */
    /*
     * NOTE: TI-RTOS examples configure pins PD0 & PD1 for SSI2 or I2C7.  Thus,
     * a conflict occurs when the I2C & SPI drivers are used simultaneously in
     * an application.  Modify the pin mux settings in this file and resolve the
     * conflict before running your the application.
     */
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);

    GPIOPinConfigure(GPIO_PD3_SSI2CLK);
    GPIOPinConfigure(GPIO_PD2_SSI2FSS);
    GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);
    GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);

    GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1 |
                                    GPIO_PIN_2 | GPIO_PIN_3);

//    /* SSI3 */
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI3);

    GPIOPinConfigure(GPIO_PQ0_SSI3CLK);
    GPIOPinConfigure(GPIO_PQ1_SSI3FSS);
    GPIOPinConfigure(GPIO_PQ2_SSI3XDAT0);
    GPIOPinConfigure(GPIO_PQ3_SSI3XDAT1);

    GPIOPinTypeSSI(GPIO_PORTQ_BASE, GPIO_PIN_0 | GPIO_PIN_1 |
                                    GPIO_PIN_2 | GPIO_PIN_3);



    EK_TM4C1294XL_initDMA();
    SPI_init();
}

  • Hi Ryan,

    Can you use the instrumented driver library and enable logging? Then do the SPI2->SPI3 setup (which works) and look at Tools->ROV->LoggerStopMode->Records to see the driver log messages. (note: the driver puts the records into the "main" logger). You can compare that to the SPI2->SPI3 setup and hopefully get some more insight.

    Here are the changes needed for the enabling the logging in the .cfg file. It's turning on kernel logs also.

    BIOS.logsEnabled = true;
    //BIOS.logsEnabled = false;

    //driversConfig.libType = driversConfig.LibType_NonInstrumented;
    driversConfig.libType = driversConfig.LibType_Instrumented;

    var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup');
    LoggingSetup.mainLoggerSize = 4096;
    LoggingSetup.sysbiosLoggerSize = 4096;

    Todd
  • Hi ryan,

                After going through your thread i found that your problem is different than mine. I was using same DMA channel for SSI1 and SSI0. But you have different channels for each SSI. I have added below faulty ssi configuration and how to solve it.

        {

           .baseAddr = SSI0_BASE,

           .intNum = INT_SSI0,

           .intPriority = (~0),

           .scratchBufPtr = &spiTivaDMAscratchBuf[2],

           .defaultTxBufValue = 0,

           .rxChannelIndex = UDMA_SEC_CHANNEL_SSI1RX,      // Same channel for SSI1 and  0

           .txChannelIndex = UDMA_SEC_CHANNEL_SSI1TX,      // Same channel for SSI1 and  0

           .channelMappingFxn = uDMAChannelAssign,

           .rxChannelMappingFxnArg = UDMA_CH10_SSI0RX,      // Same channel for SSI1 and  0

           .txChannelMappingFxnArg = UDMA_CH11_SSI0TX         // Same channel for SSI1 and  0

       },

       {

           .baseAddr = SSI1_BASE,

           .intNum = INT_SSI1,

           .intPriority = (~0),

           .scratchBufPtr = &spiTivaDMAscratchBuf[3],

           .defaultTxBufValue = 0,

           .rxChannelIndex = UDMA_SEC_CHANNEL_SSI1RX,      // I have changed these channels with diffent DMA channels

           .txChannelIndex = UDMA_SEC_CHANNEL_SSI1TX,      // I have changed these channels with diffent DMA channels

           .channelMappingFxn = uDMAChannelAssign,

           .rxChannelMappingFxnArg = UDMA_CH10_SSI1RX,       // I have changed these channels with diffent DMA channels 

           .txChannelMappingFxnArg = UDMA_CH11_SSI1TX         // I have changed these channels with diffent DMA channels

       }

    };

    Regards,

    Digvijay

  • Thank you Digvijay and Todd,
    This resolves my issues and it works on the Launchpad. It's interesting that even though I don't use SSI0 and *shouldn't* have a udma conflict, I still need to change the channel. In my case, I changed SSI1 to 24 and 25.
    Thank you!
    Ryan