This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Choosing the right driver for a DD turntable

Other Parts Discussed in Thread: DRV10974, DRV10963, DRV10964, DRV10970
Question:

I need a BLDC Driver with following parameters:
Current: 12V 
sensored or sensorless
sinusodial drive (!!!)
target rpm 33-78 (turntable)

Motor data:
Turns:110T
Poles and slots:36N42P
Wire:0.24mm
Ri(ohm):15.0ohm
Any suggestions?