This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8316: Current sensing question.

Part Number: DRV8316


Hi,

The customer wants to calculate the current value flowing through U, V, and W when the motor is driven as the phase changes.

When operating the motor, calculate the IoutA value using the formula below.

Duty = 25%
U - SOA = 1.665V / Vref = 3.335V / gain = 0.15 / IoutA = -0.00125A

Duty = 50%
U - SOA = 1.665V / Vref = 3.335V / gain = 0.15 / IoutA = -0.00125A

Regardless of the Duty value of the motor, the same value is output to the SOA and Vref, resulting in the same IoutA value being calculated.

In this case, the voltage value of outA is large when Duty is high.

Is it normal for the motor to produce the same current value because the voltage output to outA is different, but the SOA and Vref values are the same?

In addition, SOA and Vref values change little regardless of motor operation and duty.

Please give us a guide on how to sense the current of each U, V, and W.