Hi Team,
Our customer would like to set the current limit of the device to 1A. To test the current limit, he will connect resistors to AOUT1 & AOUT2 and BOUT1 & BOUT2 such that the current is slightly above 1 Amp. Then he will connect the device to a 10V power supply. He would like to know if the current limit is exceeded does the nFault pin goes to logic low and does the AOUT1-2, and BOUT1-2 go to a high impedance state?
Regards,
Danilo