Other Parts Discussed in Thread: DRV8302, DRV8353
Hi,
I thought i would start a new thread ... my old thread was DRV8302: failure of drive chip when running.
i can now run a motor but my current sense is not very good... Should i have filtering from drive chip to my micro i can see on the dev. kit that there is 56ohm and 2200pf. With what i have round me i've tried 62ohm and 1000pf but my waveform hasnt changed much.
picture shows loaded up motor pulling nearly 5A at 12v i'm using a 0.001 ohm current sense but with 33ohm in line of the op amp lines and a 10nf between (ive also tried it with these out). I'm thinking my choice of current sense is too small (i'm set at 40v/v) gain as well
blue trace - to dspic
yellow trace - h-bridge out to motor (the live side )
Also were driving the motor at 16khz ... this was set by my predecessor using the old chip and i've left it.. Is there anything stopping me going up in frequency ? or is it an EMC thing
Suggestions ?? i'd be grateful.
i'll be re-reading the application notes and data sheets over the weekend
John