Other Parts Discussed in Thread: DRV2604
Hi Arthur-san,
This is related the following E2E session.
Customer try to consider about open loop. because they cannot find solved method for the issue with closed loop setting.
Could you please review the customer setting for open loop? (frequency = 163Hz)
<DRV2604L>
・0x1A[7] N_ERM_LRA: 1
・0x1D[0] LRA_OPEN_LOOP: 1
・0x1F[7:6] AUTO_OL_CNT: 2 ※Default
・0x1F[5] LRA_AUTO_OPEN_LOOP: 0 ※Default
・0x1F[4] PLAYBACK_INTERVAL: 0 ※Default
・0x20[7:0] OL_LRA_PERIOD: 3E=163Hz
・0x22[7:0] LRA_PERIOD: 3E=163Hz
<DRV2604>
・0x1A[7] N_ERM_LRA: 1
・0x1D[0] LRA_OPEN_LOOP: 1
・0x22[7:0] LRA_PERIOD: 3E=163Hz ★
★ DRV2604L has address 0x1F and 0x20, however DRV2604 doesn't have those address.
In case of DRV2604-null, how should they set the frequency setting? Is it OK, address 0x22 only?
Thanks
Mukuno