Other Parts Discussed in Thread: DRV832X, DRV8323, DRV8353
Hello Sir,
My customer’s product is an electric power tool. They now use A4915 on their products.
The specification requirement of their motor Driver IC is that they only need to send one PWM signal to operate. Sometimes the peak current of the MOSFET (ID) can reach 60A~100A.
The customer's BLDC is 18V or 36V.
I introduced DRV8306 to the customer, and he replied that the gate driver current of DRV8306 is only 15mA and it is not enough. He hopes to be at least 650mA and preferably above 1A.
Does TI have Motor Driver products that meet customer specifications?
Best Regards,
Kami Huang