This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are using 2 stepper motors with DRV8711 with mosfet CSD88537ND. After setting up the various parameters of the driver IC as per our requirement, we are facing the issue of predriver fault and undervoltage lockout fault. Sometimes it will make 1 or 2 revolutions before the fault and sometimes it will only rotate for a tiny amount and fault appears. Each time when we clear the fault and the motor will begin to turn and then the fault will trigger again.So please provide me with the solution to troubleshoot this problem.
Hello, Shreena,
I saw several threads about this issue. Let us step by step fix this issue. First, under voltage lockout issue. After the input voltage is stable. And then, we can check the pre-driver fault.
The debugging idea and process can be found in:
(+) DRV8711: DRV8711DCP Mode selection - Motor drivers forum - Motor drivers - TI E2E support forums
If you find something, would you join the first link? So, everybody is on the same page.
Regards,
Wang Li