Other Parts Discussed in Thread: DRV8350
Hi Team,
Good day! Posting this in behalf of the customer. Here it is.
I recently switched from using the DRV8350HRTVT to
the DRV8350RHRGZR on a brushless motor controller board.
I designed a board using the DRV8350RHRGZR to drive a brushless motor but
the motor is not spinning.
I supplied 15V to the 15V inputs on the schematic, 5V to the 5V input on
the schematic, and 3.3v to the PWM and DIR pins.
I measured the fault pin (pulled up to 5V) and it reads 5V. I measured the
DVDD pin and it reads 0V.
I am using a maxon EC 45 flat Ø42.9 mm brushless motor with hall sensors.
I followed the example circuit provided on the datasheet excluding the buck
converter (because I supply 5V from outside)
Here is the datasheet:
https://www.ti.com/lit/ds/symlink/drv8350r.pdf?HQS=dis-mous-null-mousermode-dsf-pf-null-wwe&DCM=yes&ref_url=https%3A%2F%2Fwww.mouser.com%2F&distId=26
I tried connecting the VM pin to the VDRAIN pin but the motor did not spin, and DVDD pin still reads 0V.
any help would be appreciated,
Best regards,
Jonathan