This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8434: Regarding trip current accuracy vs DRV8881E

Part Number: DRV8434
Other Parts Discussed in Thread: DRV8881

Hi support team.

My customer asked me regarding trip current accuracy.

Which is better for trip current accuracy compared to DRV8881E in the following settings? (Use the same stepper.)
The error of the resistor that sets VREF is the same for both.

Full scale current setting: 400mA or 410mA

-DRV8881E settings
Sense resistance: 0.3Ω ± 1%
TRQ = TRQ = L (100%)
TOFF = 10us
DECAY = Smart tune or Mixed

-DRV8434E settings
TOFF = 7us
DECAY = Smart tune or MIxed

Best Regards,

Higa