This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8432EVM: Had noise issue for DRV8432EVM test

Part Number: DRV8432EVM

Hi Team,

Had noise issue for DRV8432 EVM test:

  1. Using a resistive load (cement resistance), when the input is 100%, the output noise.
  2. Using motor load PWM_A=100% or PWM_B=100% can work normally, but the noise is bigger

  1. DRV8423 EVM test point.docx