Part Number: DRV8812
Hi Team,
My customer is planning to use DRV8812 in one of the medical project and having below queries to proceed. Can you please help address below queries.
1) Does the pins (AI1, AI0, BI1, and BI0) control the motor current as well? Planning to have a dedicated circuit for Vref generation(different ref voltages) and sense resistors connected. Does these pins AI1, AI0, BI1, and BI0 do the same job as Vref circuit does? Currently used a DIP switch to configure the current scaling settings. See below,

2. Fault condition: Can you provide suggestions on how to implement a self-recovery circuit during a fault condition? In case of a fault condition , can the nFAULT pin be connected to RESET pin with a RC circuit (as OCP time we understand is 3.8ms, we can have a RC ckt for greater than this duration).
3. Can the signals like NSLEEP, DECAY and RESET and Bridge control setting pins( AI1, AI0, BI1, and BI0) , PHASE and ENABLE can be connected to a 5V through a pull-up?
4. VREF: As per the recommended Operating conditions, VREF has a min of 1V. Less than this will have the accuracy degraded. Question: What is the worst case voltage level where the voltage degradation will affect the system performance? (Design constraint is current control <1V VREF)

Regards, Shinu.