This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316A: Maximum motor power

Part Number: MCF8316A


We have a 24 V motor system that we need to drive at 6 A. The part specs seem to indicate this is possible, but in the forums I found mention of a 70 W input power limit. This is so far from the 35 V, 8 A spec.

Why is this not called out in the datasheet. Is it an errata? Are there any workarounds? Doesn't seem like there is a thermal reason for this limit.