Other Parts Discussed in Thread: DRV8323, , BOOSTXL-DRV8323RS
Hello TI people.
Sadly I recently burnt an evaluation board while doing a test in a 250W BLDC motor. The test was designed to stress the system forcing it to do repeated heavy accelerations.
The board has the following damages.
- GLC shorted to GND
- GHB shorted to GND
- GHA shorted to GND
- The mosfet temperature was 95°C when the evm broke down.
- No visible damage
The half bridges test all ok. So most probably the gate driver is burnt.
I'm driving the motor with the driver in 6xPWM mode, sending 6 SVMPWM with a dead time of 200ns.
The driver is set to 100ns dead-time and the default IDRIVE setting (120/240mA).
I'm supplying 40Apeak, 20A nominal current from the battery at 42V.
So my question is how come I burnt the evaluation board? What happens if the MCU deadtime is different than the one the driver is putting? Why did these gates get shorted?
Please help me try to figure out the issue.
Thank you in advance.