Team,
Customer is trying to debug an HW failure on MCT8316Z0TRGFR that seem to be related to the on-chip Buck regulator.
Only a small percentage of the boards are affected.
The behavior seen is as below:
-The Buck is used in inductor mode.
-The Buck outputs is outputing appr. 1V instead of the expected 5V (as programmed via pull-up on VSEL_BK pin).
-The IC shows a significant overheat compared to the one that work correctly.
I will provide more info off-line (schematics, IR pictures).
Can you please help to debug the behavior further in order to find the route cause?
Can you please review the schematics?
We have seen already the related Buck FAQ here.
Thanks in advance,
A.