Other Parts Discussed in Thread: DRV8311,
I would like to inquire about the PWM frequency support of the DRV8316 driver, specifically why the BLDC Integrated MOSFET Thermal Calculator lists the maximum supported frequency as 75kHz, while the DRV8311 supports up to 200kHz. According to their respective datasheets, both drivers are capable of handling up to 200kHz. Is there any difference between the DRV8316 and DRV8311 drivers that would limit the PWM frequency of the DRV8316 to 75kHz in practical applications?