This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316AEVM: MCF8316AEVM: Won't connect to PC

Part Number: MCF8316AEVM

Hi Experts,

Good day.

My MCF8316AEVM could not connect to my PC. I use MCF8316AEVM GUI to connect MCF8316AEVM via USB, the power is 12V. The Gui always shows connecting to the target, but can't connect my device. The  D1, D4, and D6 LEDs are on.

I did follow the MCF8316AEVM: No detection of EVM
(1) download the offline installer, but I don't know how to open offline Gui, or it just is installed and doesn't need to be opened?
(2) D1 ,D4 and D6 LED is on
(3) uninstalling the TI Cloud Agent and installing again, launching the GUI in your web browser again.
MCF8316AEVM also can not be connected, it always shows installing the Windows driver


Please advise

Regards,

Josel