Hi team,
The customer would like to test the brake functionality when debugging the MCT8316ZR chip.
Set Control_Register_7 Register, branch_mode = 0, brake = 1.The brake pin is set high through MCU, the drvoff pin is set to 0, and the nssleep pin is also set to 0. When the brake pin is low, the motor can be controlled to turn. When the motor stops, the brake pin is set high and the motor cannot be held. Why's this?
Could you help check this case? Thanks.
Best Regards,
Cherry