Hi,
I am using DRV8844 to drive 2 valves right now and it works as expected.
I am planning to add 2 additional heaters, schematic as below.
As I understand the datasheet each pin OUT1..4 can support 2.5A also the VM is directly connected to the mosfet internally to the IC. So the VM is getting redirected to the fets.
The valves on out 1 and out 2 consume around 400mA together
The heaters on out 3 and out 4 will consume around 1.5A.
All these outputs will be on at the same time. I wanted to know if the IC itself can handle all the pins with high current at the same time.
For example Vm = 24V and Combined current of OUT1..4 = 10A
If so apart from adding in wider traces is there anything else which needs to be considered like hear dissipation etc?
Schematic
Heater specs
Thank you,
Bhavya