This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8412: Schematic Review Request for driving a thermoelectric heater/cooler (Peltier)

Part Number: DRV8412
Other Parts Discussed in Thread: DRV8962, DRV8952, DRV8262

Hello,

   I have an application where I need to drive a thermoelectric cooler, both for heating and cooling. 24V nominal. Current is 4.5A typ, 5.4A maximum. I will be driving it with PWM, frequency TBD but probably as high as the DRV8412 can go (500kHz) to minimize output filtering.

   Also in this design is high level current sensing using an INA180A2.Thermoelectric.pdf

Thanks,

Derek