Hello.
I am testing DRV8353H in 1xPWM mode.
VM = 15V
VDRAIIN = 24V
For testing purpose, I am using function generator to generate the PWM at 10KHz.
The bulk capacitance at MOSFET supply is around 300uF, motor is taking <1amp current at no load during free run.
I power-up DRV circuit first and then turn-ON the PWM - everything is fine and motor starts to spin.
DRV circuit power down first and then PWM turned-off - no problem
But if motor is running and PWM is turned off before DRV circuit, after 2 to 3 times, following problem occurs.
VGLS goes down to ~4 volts.
DRV current increases to ~120mA.
IC starts to get hot.
I have to replace the IC to get the circuit working.
Why is this happening?
Is BEMF destroying the IC? It has the path to go to the MOSFET supply.
Regards.