Currently we are using DRV8308 to control Blower "Brushless DC Motor" to control air flow the motor is working smoothly and transitions is smooth
- our main problem now is Rise and Fall time while changing speed we are using Driver register to control motor speed and it takes about 600 ms to change speed from 0.2 to 0.8 of full speed
we tried to modify driver registers and adjust settings but without any success time transition still the same
is there any configuration or settings to reduce that time we need it to be less than 100 ms?