This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305: Unclear Gate Timing

Part Number: DRV8305


Hi together,

I have two follow up questions to my original question regarding the timing of the DRV8305 Gates.

It was: Could the parameters  t_pd_if-O and t_pd_ir-O be the time between INH_x rising/falling and the low side gate GLS_x rising/falling?

So my follow up questions are

How can the parameters t_pd_if-O and t_pd_ir-O be typ. 200ns while the minimum dead time t_d_min is typ. at 280ns which doesn't include the configurated dead time t_dtp?

I'm questioning this because Figure 11 in the datasheet shows that there is at least the dead time between INH_x rising and GHx rising (See screenshot below).

Thanks in advance