Hello
i want to use DRV8353FS. I need to simplify the BOM as much as possible. Can you please tell me if using 10K pullup resistor on SDO is ok or i must use 1K resistor.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
i want to use DRV8353FS. I need to simplify the BOM as much as possible. Can you please tell me if using 10K pullup resistor on SDO is ok or i must use 1K resistor.
Thank you
Hi Mirza,
A 10K pullup can be used instead of 1k. We typically recommend 1k-10k, so as long as it is within the range it will be okay.
Best Regards,
-Joshua