This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8962: Single BDC control with the DRV8962

Part Number: DRV8962
Other Parts Discussed in Thread: DRV8262

In the DS one of the options is to connect only one BDC motor to the driver, while in the EVB the motor and EN/IN  are somehow different, can I connect the EVB to a single BDC motor and how can I control it through the App ?  

  • Hi Shai,

    Please refer to the EVM top view image in page-44 Appendix A of the EVM User's Guide. You can remove the jumper shorts indicated by red X in the below snippet and bridge the connections shown by the solid red line. After this modification you can use EN1 and IN1 & EN3 and IN3 controls in the GUI app and drive the device. 

    We also have another variant of this product DRV8262 which has native support for paralleling two H-bridges for a single H-bridge operation. 

    Regards, Murugavel