This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8243-Q1: Maximum load inductance requirement.

Part Number: DRV8243-Q1

What is the maximum load  inductance that can be connected to DRV8243 and DRV8245?

  • Hi Pratik,

    Thank you for your post. Could you please elaborate the nature of the load in your application? Is it a BDC motor or some other type of load? The DRV8243-Q1 is a fully integrated full-bridge driver. All electrical characteristics of a full-bridge driver applies to this device. We have published absolute maximum ratings and recommended operating conditions for this driver. As long as these specifications are not violated in an application the device should drive any type of load. If you have a specific requirement please share more details such as operating voltage, target current, PWM input and duty cycle needed, inductance of the load, DC resistance of the load, type of load etc. We'll try to provide information pertaining to that. Thanks.

    Regards, Murugavel