This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605: HAPTIC Reactor Heavy device

Part Number: DRV2605

Hi Sir,

My customer is surveying the DRV2605, could it support driving the below HAPTIC Reactor Heavy device? Thanks!

product_spec_afr14a901b_zh_hans_49f862c1b8.pdf

  • Hello,

    Thank you for reaching out. Please expect a response by the end of the day. Thank you.

    Regards,
    Sydney Northcutt 

  • Hello,

    The resonance frequency of the actuator is 120Hz where as the LRA frequency range for DRV2605 is 125Hz - 300 Hz. Our devices also aren't really designed for actuators with such large acceleration (8G) as the BEMF would likely be too high for auto resonance tracking to work here even if the resonance was within the device range. This actuator should work with this device in open loop mode though. 

    Regards,
    Sydney Northcutt