Part Number: DRV10983-Q1
Hi Team,
1) Can the DRV10983Q1 set the PWM operating range? Now only the lowest duty cycle setting is seen, below 5% is output at 5% and below 1.5% is output at 0. Is there a maximum duty cycle setting that allows it to output at maximum speed above 98% duty cycle?
2) Can the PWM set the correspond actual speed? For example, 30% duty ratio should be 1000 rpm.
3) What is the general time for the motor to start up? Set the 1st and 2nd order acceleration to a maximum of 8 seconds to reach the target speed.
Could you help check this case? Thanks.
Best Regards,
Cherry