Other Parts Discussed in Thread: MSP430FR2355, MSP-EXP430FR2355, MCX8316AEVM,
Hi Team,
The customer follows the description in the guide, connects the hardware, and connects the 10V power supply between VBAT-PGND. Then uses the Micro-USB cable to connect the computer and evaluation board. A green light appears on the GUI graphical interface. The lower left corner shows that the hardware is connected and the serial port baud rate is 9600. At this time, he clicks Read All Registers and waits for more than three minutes, but no read register is displayed and the D6 indicator light does not light up.
Best regards,
Annie Liu