This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-DRV8323RH: Chip generates heat when running under load

Part Number: BOOSTXL-DRV8323RH


Hi Team,

The DRV8323RH motor driver chip is used. When the motor continues to operate with a load power of 180W, the temperature of the DRV8323RH chip rises very quickly. The temperature reaches about 80 degrees in about 10 minutes, and then stabilizes when the temperature reaches 103 degrees. Why does the temperature of the DRV8323RH chip behave like this during operation? The IDRIVE setting is 570/1140 mA, and the VDS setting is 0.26 V.

Reagrds,

Annie