This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The datasheet for LMD18200T/NOPB includes two different variants of the circuit, both called "NDJ" package. One that is vertical (NDJ0011B/TA11B) and one horizontal (NDJ0011E/TA11E).
On page 2, it references NDJ0011B. However, when looking at the available symbols/footprints, the 3D model for included for TA11B is the horizontal one, but the footprint seems to indicate that it is for the vertical one.
When I order the part will I get a vertical och horizontal component?
And for the vertical, is the 3D model available anywhere?
Best Regards
Hey Nilsson,
See below images. Order package E (LMD18220T/LF14) to receive horizontal version. Sorry for the CAD model confusion, I'll work on getting that fixed!
Thanks,
Jacob
Hi,
Thank for the info, but how do I see that the LF14 corresponds to NDJ0011E. The order code in the datasheet says package name is just NDJ for both devices:
/PA
Hey PA,
Unfortunately at this time you just have to trust me, we're working on updating the online info but it's taking longer than expected. I pulled the below quote straight from an email with our packaging team where we discussed the changes to implement:
LMD18200T/NOPB should be NDJ0011B
LMD18200T/LF14 should be NDJ0011E
Best,
Jacob