Hi. I tried to connect DRV8706S-Q1EVM(MD023B) to the GUI but it is not working. Board is powered with 12V and status LED is flashing(LED D5 is flashing, LED D4 is on, LED D3 is on.). GUI is also automatically trying to connect after USB plug in --> Result: Hardware not connected.
I followed the guidance in this link but it didn't work. e2e.ti.com/.../drv8706s-q1evm-unable-to-connect-gui-to-eval-board
I tried the both cloud-based GUI version 0.5.5 and 1.2.2 as well as downloaded GUI version 0.5.5.



I'm sure to click the appropriate variant selector box. And I installed the drivers in the picture below(VCP Drivers, D2XX Drivers). But it still shows that hardware not connected. Could you pls help me?