This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323: Block BLDC Motor using DRV8323 in 1XPWM mode

Part Number: DRV8323

I am operating a BLDC motor using DRV8323 motor driver in 1 X PWM mode. After my motor stops, it remains free and can be moved by external mechanical force. But I want my motor to get hard locked/jammed when it stops. I tried doing this using brake bit in driver control register but it is for stopping the motor not for locking or blocking it. 
If I could get a help here. 
Thanks in advance.