In the case of stepping on and stepping deeply, the high current passes through the drive bridge, and the fault is reported DRV8343, and the current sampling is abnormal after the shielding fault is tested, which is suspected to be a problem inside the chip. Report fault information such as attached pictures, help see what is the reason? How to solve it?