Part Number: DRV8306
Other Parts Discussed in Thread: DRV8320, DRV8328, DRV8323, DRV8329
Hello Team,
we have already developed BLDC driver using DRV8306 for normal linear operation. we want to upgrade the design by including below features in it.
1. oscillation mode- motor should able to oscillate from 200rpm to 20k rpm
2. Position control using incremental and absolute encoder feedback
can above feature will be able to achieve using DRV8306 , if not please suggest another IC and also which commutation we need to used.
do you have evaluation board which can have similar function.
Regards,
Sayali