This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8329: CSAGAIN Setting

Part Number: DRV8329

hello, 

I am using DRV8329 to spin 3 Ph BLDC motor on one of our Project. this is a key project we are working and has very high annual volume ( > 50k)

we are evaluating the possibility of using CSAGAIN and SO pin to read the current from Motor and have Connected CSAGAIN To GND to read max current. Peak current (motor phase) in my application could go up to 90A during startup at load. 

I am getting good data on the SO Pin but the voltage does not match with gain mentioned in the datasheet. 

 

with CSAGAIN to GND I calculated table in above image. below are scope captures of Motor Phase current peak value and SO pin voltage wrt GND. there is clear offset of 400mV to 800mv which is very high. see below captures for reference 

Peak current at startup is 81A, according to table, SO Voltage should be close to 1.24V but i am seeing 1.92V here, some more images below during operation 

Request you to provide some feedback on the discrepancy observed. Below is snapshot of DRV8329 section.