This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305: DRV8305N used in In-phase current sense application.

Expert 1215 points
Part Number: DRV8305

Hello,

I am using DRV8305N in my Motor Control Application.

So far I was using Low-Side Current sensing and integrated CSA's in DRV8305N.

Now I redesigned a little my project to have external CSA (INA241) and In-Phase Shunt resistors

It was only this change, current sensed by INA seen at ADC is corrected (checked it), but DRV is giving errors/damaging.

This is stragne because nothing apart way of current sensing changed and current sensing itself is workign correctly looking at the ADC valuse.

I have SNx/SPx Inputs left floating and all SL_x (so source of low-side) are now (in case of lack of low-side shunts) tied to GND like in the picture:

Can DRV work in that configuration? I am debugging the problem but maybe some has some suggestion what could be the problem?

Regards,

Adam