This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353R: GLC and SPC getting shorted with 48V Motor

Part Number: DRV8353R

Tool/software:

Hi

I have a motor controller for a 48V PMSM motor using DRV8353RSRGZR.

Some of the boards are having problems with the DRV8353RS that the GLC and SPC pins were shorted to each other and  GND pin, and the mosfet connected to GLC is fine .

I don't know the conditions on which those boards were damaged.

I just want to know what can damage the GLC and SPC and what can I do to avoid this happening to other boards.

I have all ready shared the schematic and PCB layout to TI FAE.

Please provide the solution.

Thank You,

Shambhu