Tool/software:
I am bringing up a new design using the DRV8328 and running into an issue with certain setups that will cause the MOSFETs to burn.
I thought this was due to the switching times being too fast, so I increased the gate resistors to 100 Ohm instead of the 18 in the schematic. That increased the Vds fall times from 40ns to 180ns. My dead time is around 2000ns.
Even after switching out the gate resistors and increasing the dead time, MOSFETs are still burning up. Under no to light load.