This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8452: Kv constant and Max Vref,

Part Number: DRV8452


Tool/software:

Hi ,

for DRV8452, there are two package available, do they both have Kv=0.66?

 DDW Package: 5 A full-scale, 3.5A RMS 

 PWP Package: 4 A full-scale, 2.8A RMS

IFS *Kv= Vref, KV=0.66, 

for PWP package:  Max Vref = 4A*0.66= 2.64V