This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353:DRV8353SR芯片使能后,PWM未输出情况下,报fault错误问题

Part Number: DRV8353

Tool/software:

您好,我们在使用DRV8353SR时,测试发现有两个问题

下图是驱动A相的电路图,MOS的Qgd为12~18nC

1.板1在三相输出悬空时,SPI按默认配置,直接配置使能芯片EN,MCU输出3相互补的16KHz的50%占空比PWM,mcu设置死驱1us,测试前几次能抓取A,B相输出PWM,频率及死驱基本能对上,测试几次后,fault寄存器报0x620,A相上管VDS过流,将A相PWM关闭,B,C相PWM能正常输出,同时测量SHA对GHA的二极管电压为1.632V,而B相和C相均为0.567V,GHA对SHA电压为1,这是否说明内部二极管已经损坏了?三相悬空时驱动电流过大是否是造成此次损坏的原因?

2.在测试另一块板时,同样在三相输出悬空,且MCU的PWM不输出情况下,同时SPI配置DRV8353S的drive电流均设置为最小,在给到DRV8353S 使能信号大约16us后,抓取到fault上有一低电平,抓取波形如下图所示,CH1为给到DRV8353的EN信号,CH2为fault信号,CH3为VM电平, 此跌落在其他板上未抓取到,后经过SPI读取fault寄存器,确认报错为0x700,但此时MCU的PWM均未输出,gate driver fault condition这个错误如何进行排查,另外为何还会报VDS过流?