Other Parts Discussed in Thread: DRV8873, , SN74LVC8T245-EP
Tool/software:
Subject: Urgent Help Needed: Issues with DRV8873-Q1 H-Bridge Driver in Project
Hi Team,
We are currently integrating the DRV8873-Q1 H-bridge driver from TI into our project as an alternative to the VN771K for obsolescence management. Each board uses 8 H-bridge drivers, and we are encountering several issues during board bring-up. I’ve attached the board schematic, connection details, and datasheets for your reference.
Here are the issues we’re facing:
-
Shorting of DVDD and GND Pins: We are observing a short (around 5.6 ohms resistance) between the DVDD and GND pins in the H-bridges. This issue has been noted in 15 units so far.
-
Level Translator IC Failure: The SN74LVC8T245-EP level translator IC has failed while driving the load.
-
Output Voltage Spike: A spike with an amplitude of nearly 28V is observed at the output side of the IC when the load is connected and driven.
-
nFault Pin Behavior: The nFault pin goes low after approximately 25 seconds of power-up. Should we reset the sleep pin to clear this fault?
-
Damage to DVDD Due to VM and GND Short: If the VM and GND pins are shorted due to glitches at OUT1 and OUT2 (Ref:picture1:- glitch observed at outputs, picture 2: waveform at OUT1 and OUT2 pins), could this damage the DVDD output? If so, what is the maximum duration of such a glitch that can cause damage? The chip is configured in the hardware PWM mode and driving the OUT1 and OUT2 with 600 ms time gap
HBD SCH.pdfRelay datasheet.pdf
We are looking for suggestions on debugging these issues and ensuring the boards are ready for production .
.
Thank you for your assistance!