Tool/software:
Hi,
Referring to the "Related Questions", I wrote firmware (MCxGUI_Comm_Bridge_MSP430FR2355_v0.0.9.out) to the MSP-EXP430FR2355.
Writing to the MSP-EXP430FR2355 using the desktop version of UNIFLASH was successful. However, when I then connected P4.6 of the board to the target's SDA, P4.7 to the target's SCL, and GND to AGND, and started up MotorStudio, it was not recognized as shown in the figure below. The target board is equipped with an MCF8316A. Can you give me some advice?
Thanks,
Conor