This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
I am using the haptics driver (DRV2625) with the evaluation board (DRM2625EVM-CT) to get preliminary haptic vibration data. The problem that I am having it after the system is connected and I have successfully drove the haptics motor, I am not able to put sequences in a series or add any delay between the sequences. See the highlighted section in the photo attached. Any ideas how I can fix this problem?
Example of my goal: strong click -> delay 6ms -> transition hum 1 -> delay 3ms -> soft fuzz
Thanks all!!
Claire,
Thanks for reaching out. Your question has been received. I will get you back as soon as possible, usually within 24 hours.
Best,
Hailong
Hi Claire,
I looked at your question. Did you try click on the ON/OFF in your red rectangle? You should be able to add a sequence by click 'on' first. Let me know if it doesn't work.
Also, the delay duration can be set at a minimal of 10ms in the GUI, not 6ms or 3ms.
Thanks
Hailong
Hi Hailong,
Yes I have tried clicking on the ON/OFF. When I clicked start there was no response from my motor. What else can I do to fix this?
Sincerely, Claire
I just tried to turn one on delay and still there is no response from the haptics motor.
Hi Clarie,
Please refer to the setting below. The sequence will be: strong click -> delay 10ms -> transition hum 1 -> delay 10ms -> soft fuzz.
Let me know if you have additional questions.