Tool/software:
Hi,
If I'm not using the internal DC-DC converter of the DRV8350RHRGZ, is it okay to connect all pins to GND?
Or, since VCC is the internal regulator output, in order to maintain stable operation, should I not connect the VCC pin directly to GND, but rather connect a 0.47 µF capacitor between the VCC pin and GND?
Please comment on what I should be careful about when handling pins when not using the internal DC-DC converter.
Thanks,
Conor