Other Parts Discussed in Thread: DRV8873, DRV8145-Q1
Tool/software:
Hello,
I wonder if it is possible to connect multiple outputs or entire DRV8873 modules to increase the load current?
For example, combining two outputs OUT1 and OUT2 of one DRV8873-Q1 system and high-side control to increase the maximum load current.
Or connecting two separate DRV8873-Q1 modules in parallel?
Best Regards,