Other Parts Discussed in Thread: MCF8329A
Tool/software:
If I change the jumper from position 1-2 to position 5-6 in J12, after sometime the I2C is automatically disabling but no faults from driver or controller.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
If I change the jumper from position 1-2 to position 5-6 in J12, after sometime the I2C is automatically disabling but no faults from driver or controller.
Hi Babji,
If the jumper on J12 is moved from position 1-2 to position 5-6 the source to VREG changes from AVDD to the external MOSFET (Q7). The external MOSFET requires R56 to be populated with at least a 0 ohm resistor so that GCTRL can be used to provide control to the gate of the MOSFET. Without GCTRL being connected to the MOSFET, VREG does not receive 3.3V which means the digital core of the MCF8329A is not powered.
R56 was depopulated since when VM is set higher than 40V, R56 is populated, and J12 was not in position 5-6 the GCTRL pin can become damaged.
To use position 5-6 of J12, you will need to populate R56 and we recommend to not move the J12 jumper to prevent device damage while R56 is populated.
Regards,
Joshua
Hi Joshua,
R56 is still there. I didn't depopulated. But still the issue is there.
(after sometime the I2C is automatically disabling but no faults from driver or controller).
Can you provide a capture of the voltage on DVDD, VM, AVDD, and the SPEED/WAKE pin starting from when the device is fine to when I2C is disabled?
Also can you check what the value of DRV_MODE in DEVICE_CONFIG (0xAA) while the device is active? If this is set to 1b then the device may be going into sleep mode.
Regards,
Joshua