Other Parts Discussed in Thread: DRV8703-Q1
Tool/software:
Is it possible to set the current limit while operating in Independent Half-Bridge mode (PMODE = open)?
Section 7.3.2.3 says that internal current regulation is disabled in independent mode, but in that case what happens if the output is shorted?
Ideally I would like to operate the device in independent Half-Bridge mode with a maximum output current limit set to 100mA (the actual current will be < 10mA). Is that possible with this device?
If current limiting is not possible, what should be done with VREF, IPROPI, and IMODE pins?